(3)| 6/28/2010 2:07 PM | |
|
Posts: 122 Rating:
|
Hi everyone! I'm trying to simulate the tags in my Step 7 program, which has WinCC Flexible project integrated, without having to start the WinCC Flexible Runtime. I want to set the values for tags inside instance data blocks. I don't know wether that's possible or I will need to start the Runtime in any case. I've tried to set the values in the data block while PLCSIM is running but I get an error message (I'm translating from Spanish so there might be differences with the English error message): "This function is not allowed with the current protection level" --> page1 As this was not working I tried using the variable table but when I enter the operand (which is INT type) and try to set the value I get and error too. --> page2 I'm sure I'm doing something wrong but I can't figure out what it is. Could somebody give me a hand here? Thanks in advance Sara Attachmentcapturas2.pdf (508 Downloads) |
| 6/28/2010 3:12 PM | |
|
Joined: 5/28/2008 Last visit: 1/14/2026 Posts: 4522 Rating:
|
Hello, I think the attached document will be useful. Hope this helps AttachmentPRO1_09e_DBs.pdf (839 Downloads) |
|
Ayman Elotaify |
|
This contribution was helpful to
|
|
| 6/28/2010 3:19 PM | |
|
Posts: 122 Rating:
|
Thanks for the attachment Ayman! Now I have no doubts about addressing. Now I see I had made a silly mistake... Sara |
| 11/13/2016 12:08 PM | |
|
Posts: 2 Rating:
|
check the PLC switch. it might be in RUN mode. put it to RUN-P mode. |
This contribution was helpful to
|
|
| 3/20/2017 4:19 PM | |
|
Posts: 4757 Rating:
|
New question published by Amit.kumar16 is split to a separate thread with the subject simulate the contents of a DB in PLCSim. Best regards |
This contribution was helpful to
|
|
| 4/7/2017 12:26 PM | |
|
Posts: 2 Rating:
|
AutoGen_1058531! Thank you for your help in correcting the error 33:53409! |
Follow us on