(0)| 7/27/2010 11:51 AM | |
|
Joined: 4/24/2006 Last visit: 1/16/2026 Posts: 9105 Rating:
|
Dear Ash Man, It is absolutely possible to communicate via Profibus. This link, might help: how do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7-400 via Profibus/MPI? Restriction is max. baudrate is 1,5 Mb and HSA should be less or equal 63. It is possible when you use WinCC flexible 2005 or higher. Go to connections -> parameters. On the left you see HMI and on the right PLC station. In the middle you can select Network, choose profile 'DP' Best regards, Wizard |
Last edited by: Wizard at: 7/27/2010 11:52 AM |
|
| 8/29/2017 1:04 PM | |
|
Joined: 8/21/2014 Last visit: 12/19/2025 Posts: 1098 Rating:
|
New question published by reza1376 is split to a separate thread with the subject I need a solution for doing Fixed Frequency from HMI to MM420 on Profibus . Best regards |
|
My Forum is the place to personalize your profile, |
|
Follow us on