(0)| 12/18/2010 12:27 AM | |
|
Posts: 2661 Rating:
|
Are you sure? The RSE can add the FB call only for blocks programmed in LAD, FBD or STL and not CFC. You'll get an error message as shown in the attachment. For S7 programs with CFC the RSE just adds FB49 (and FC49) to the block folder. So youhave to call the FB49 in any CFC (after inserting the FB from offline block folder to the chart folder), go to the runtime groups and copy the call to all the required OB's. Regards AttachmentDokument1.pdf (489 Downloads) |
| 12/18/2010 8:49 AM | |
|
Posts: 335 Rating:
|
Dear Phantom75, I added FB49 to all OBs that I need it.After CFC compile of my problem,I got some warnings such as: "Block FB49 contains arecursive call" and "Block OB72 contains a recursive call" and ... How can I resolve these warnings? AttachmentWarnings.pdf (449 Downloads) |
Follow us on