(6)| 3/3/2011 11:03 AM | |
|
Joined: 10/3/2010 Last visit: 1/14/2026 Posts: 1572 Rating:
|
Please do so, efka, I'm interested in this too, so your pdl would be very welcome |
|
B r g d s , |
|
| 3/3/2011 3:26 PM | |
|
Posts: 799 Rating:
|
Well, attached the pdl. NOTE: You have to create internal tag oftype "TextTag" with the name "folderpath" if you don't want to change the scripts For this tag you have to enter a start value, which contains your folder path like C:\test\ Don't forget the last backslash!!!! Feedback would be great best regards from Germany AttachmentOpen_PDF.zip (1288 Downloads) |
Last edited by: efka at: 3/3/2011 3:27 PM |
|
This contribution was helpful to
|
|
| 3/4/2011 8:45 AM | |
|
Joined: 10/3/2010 Last visit: 1/14/2026 Posts: 1572 Rating:
|
efka, thanks for attaching the PDL, I just tried it and it looks very nice. Just had to replace all texts (from ?????? to the ones from your jpg). A few remarks to remember: 1. if there are files in the folder to scan which can't be viewed in the webbrowser object, they will be opened with the according software (like Word,Excel, ...) 2. if a pdf is viewed in the webbrowser object, you can easily get access to the full system. Click on the Save-button in the top bar and the Save-dialog opens. From there, you have the Windows Explorer and you can start any executable with a rightclick instead of saving the file. Probably this can be changed by pdf viewer settings... Just to be sure, the above remarks are remarks, not complaints! |
|
B r g d s , |
|
| 3/4/2011 10:39 AM | |
|
Joined: 10/3/2010 Last visit: 1/14/2026 Posts: 1572 Rating:
|
thanks for the feedback efka, one more thing: when clicking on "Scan Folder", the last entry of the listbox is selected automatically and the webbrowser loads that file. However when you have multiple files in the folder, the webbrowser refreshes several times (probably due to updating the listbox entries and changing SelText) |
|
B r g d s , |
|
Follow us on