(4)| 3/9/2011 6:48 AM | |
|
Posts: 17 Rating:
|
Thank you so much for your response. One more thing, do you have any idea regarding the sampling rate when Profinet is used? |
| 3/9/2011 1:14 PM | |
|
Joined: 10/7/2005 Last visit: 1/22/2026 Posts: 3054 Rating:
|
Hello Aevat I use ibaPDA-S7Analyzer regularily for all sort of commissioning and troubleshooting purposes and we (I also work for ibaOceania) have a fair few customers who do the same. The advantage of ibaPDA-S7Analyzer overibaPDA-S7-TCPIP is that it is a request based aquisition and youNOT need to write any logic in the S7 PLC. If you do NOT yet have an ibaPDA system, all you have to buy to get startedis the ibaPDA-S7Analyzer which allows you to aquire 64 Tags (you can buy ibaPDA tag upgrades if you needto aquire more tags later). Aquisition speed depends on a number of factors (e.g. number of signals to be aquired, network traffic, CPU type and communciation load etc.), but expect to get update rates of typically 10ms to 30 ms with modern PN CPU's. Attached is the flyer for ibaPDA-S7Analyzerand I suggest you get in touch with your nearest iba office (see www.iba-ag.com) who will look after you. AttachmentibaPDA-S7-Analyzer.pdf (1851 Downloads) |
|
Cheers |
|
This contribution was helpful to
|
|
| 3/10/2011 12:22 AM | |
|
Joined: 10/7/2005 Last visit: 1/22/2026 Posts: 3054 Rating:
|
Hello Aevat ibaPDA-S7Analyzer is a bit of a special offer in the iba range. When you buy this package you get the "real"ibaPDA-V6 software together with the S7 Analyzer "I/O driver" and a license to aquire64 tags (plus ibaAnalyzer which is freeware for any iba user anyhow). You can "grow" this ibaPDA-V6 system later buy purchasing bigger tag linceses, adding other Ethernet "I/O driver" licenses to it (e.g. Ethernet IP for Rockwell PLC's), add ibaFOB cards to the ibaPDA-V6 PC together withBus Sniffer modules (e.g. Profibus) or hardwired PADU's (Parrallel Analogue Digital Units) etc. etc. etc. As for your other question "is ibaPDA-S7 Analyzer still ok when used for LEVEL 2?" I'm not too sure what you mean. ibaPDA-V6 (including ibaPDA-S7Analyzer) does come with a free OPC Client and Server which you can use to exhangedata witha Level2 system if that is what you are after. I hope this helps |
|
Cheers |
|
This contribution was helpful to
|
|
| 3/17/2011 4:07 AM | |
|
Posts: 17 Rating:
|
Thank you so much Fritz for the information. It really helps a lot. |
| 3/17/2011 7:18 AM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
See there referencelist.pdf
Currently I am using iton 5ms. Best regards, Hristo Mihalev |
Follow us on