(0)| 5/20/2011 1:20 PM | |
|
Posts: 5 Rating:
|
Hi, I have just been asked to be in-charge in one of the labs at my Institution. Few months ago, battery for one of the CNC turning machines with Sinumerik 810D PLC had empty and also successfully been replaced. However, after the replacement made this machine can't function as usual again with the warning "2001 PLC has not started up " as shown below. We already called few Engineers but all of them claimed that they solve it because the "parameter" of the machine had gone. The worse is, we didn't do any backup(or don't even have any backup) for everything's due to lack of knowledge(since I just a fresh tutor) about the machine. I tried to search at this forum and found that this warning alarm can be dismissed by Clear/RESET the PLC data first, and then restore the NC/PLC achieve to the machine using WINPCIN. (Corretlyme if what I mentioned above are wrong) Now I'm confusing, what is NC/PLC achieve that mentioned? Is it just a file that I can get from SINUTRAIN(that's what we use at here to run the simulation)? Which means I just need to take one functional file and send it over the machine? I had attached two photos at below which showing the type of PLC and alarm warning that I get. Expert out there, please guide me. Thanks Regrads, Daniel Attachmentpictures.zip (827 Downloads) |
Last edited by: O_Moderator at: 5/20/2011 1:33 PMphotos transferred to attachment |
|
| 5/20/2011 2:38 PM | |
|
Posts: 2964 Rating:
|
Hello.. You can check it on OP i.e operator panel (screen what your seeing) back side this items are PCU20/MMC100.2 or PCU50/MMC103. Regards, Ekalavya |
Follow us on