2/21/2007 11:37 AM | |
Joined: 4/24/2006 Last visit: 9/15/2025 Posts: 9027 Rating:
|
[quote user="eddyqxl"] Hell: I'm using CPU414-2 for one project.But the program is too big ,now it's work memory is full.I already compressed.It's also 100%. How can I find another way to make the workmemory size smaller? Hello eddyqxl, Have you this manual: http://support.automation.siemens.com/WW/view/en/14016796 Chapter 4.1 etc. Here are some way's to extend work memory. ![]() Perhaps there are DB's you can unlink. Then they only appear in load memory. Best regards, Wizard |
12/1/2017 11:23 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8171 Rating:
|
New question published by ramatata is split to a separate thread with the subject Added new IM in to plc hadrware configuration - How much memory increased?. Best regards |
Follow us on