(0)| 11/14/2011 4:11 PM | |
|
Posts: 739 Rating:
|
Hi, If you have a CU < V4.0, please see Application http://support.automation.siemens.com/WW/view/en/22318072 This Application note is written for a MM440 and 4 pol Motor (!), but can be used for G120 with PM240 and CU240x <V4.0 [For your (6 pol Motor) applivation I suggest using a S120]. Might be the resistor is defect. I guess that you are using a standard resistor for 5% duty cycle, pls use a much bigger braking resistor http://support.automation.siemens.com/WW/view/en/22101908 |
This contribution was helpful to
|
|
| 1/14/2014 1:15 PM | |
|
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating:
|
New question splitted to how energy will be dissipated in the DBR? Best regards O_Moderator |
| 9/10/2015 1:01 PM | |
|
Posts: 4757 Rating:
|
New question published by ubiwan02 is split to a separate thread with the subject Drivers failed at deep power. Best regards |
Follow us on