12/17/2011 2:25 PM | |
Posts: 30 Rating:
|
Sir, I know this procedure in Step7 , think is currently i am using TIA V10.5 SP2, in that i dont know how to install GSD file. With regards, P.Krishnakumar
|
12/17/2011 3:05 PM | |
Joined: 9/8/2009 Last visit: 7/17/2023 Posts: 1410 Rating:
|
Manual chapter 8.1 pdf version - STEP 7 Basic V11.0 SP2 STEP 7 Professional V11.0 SP2 online version - STEP 7 Basic V11.0 SP2 STEP 7 Professional V11.0 SP2 |
This contribution was helpful to
1 thankful Users |
12/17/2011 5:05 PM | |
Joined: 8/31/2010 Last visit: 7/18/2025 Posts: 1525 Rating:
|
Hello krishnakumar, In general any DCS will act as a PROFIBUS DP master. So you can't use S7-1200 as a DP master. Still S7-1200 can act as a PROFIBUS DP Slave. You can use this module for the same: CM 1242-5 PROFIBUS DP-Slave- 6GK7 242-5DX30-0XE0 I suggest not to go for a Ethernet to PROFIBUS convertor as you have a dedicated module as DP Slave (CM 1242-5). Additonally "Use of PROFIBUS functionalities with the S7-1200 is only possible with CPUs as of firmware version 2.0." and above Also the CPUs of firmware version 2.0 is supported by STEP 7 Basic v11 / STEP 7 Professional v11. The CPUs of firmware version 2.1 is supported by STEP 7 Basic v11 SP1 / STEP 7 Professional v11 SP1. So STEP 7 v10.5 SP2 will not be useful in this case. You need the GSD for this CM1242-5 in the 3rd party DCS end, you can download the same from here.Download GSD File CM 1242-5 |
Like it? Rate it! |
|
This contribution was helpful to
1 thankful Users |
Follow us on