(2)| 1/17/2012 11:22 AM | |
|
Posts: 836 Rating:
|
Hi, you can use the process object view to get an overview of block parameters. You can apply different filters, so you can search for specific blocks. There you can also change many values in short time. Wich blocks are you using (APL, Standard, own Blocks)? The requirement is, that the charts containing the blocks are in the TH (should be in PCS 7) and that the block-inputs you are looking for are defined as "Signal" or "Parameter". If these block-inputs are not defined as "Signal" or "Parameter" you can easily do this and the use process object view. To defineseveral of block parameters as "Signal" or "Parameter" you have to do following: Go to Process Object View,select "Options > Process Objects > Select I/Os..." In this dialog you can filter, or simply display all I/Os in the project. Now you can choose wich block-I/O should be "Signal" or "Parameter". If you have forced values in you charts, you can see them by opening any CFC chart and go to "Chart Reference Data > Forced Values". There are all forced values listed. I added some screenshots of some dialogs, maybe they help. AttachmentScreenshots.zip (231 Downloads) |
This contribution was helpful to
|
|
Follow us on