(0)| 4/4/2012 6:32 AM | |
|
Posts: 38 Rating:
|
Please help me use function Position with AnalogOutput. Thanks! |
| 4/4/2012 9:30 AM | |
|
Joined: 8/31/2010 Last visit: 12/6/2025 Posts: 1525 Rating:
|
Hello thunder, When you are using the Technological Function - CPU 31xC: Positioning using Analog Output - the output from the CPU 314C can be provided only as a Analog Input for your drive. Check if this is OK for your servo application first. Then Getting started document for the CPU 31xC: Positioning using Analog Outputis available here (online version). Additionally the principle and details of CPU 31xC: Positioning using Analog Output is available here (online version) |
|
Like it? Rate it! |
|
This contribution was helpful to
|
|
Follow us on