5/21/2012 2:57 PM | |
Posts: 947 Rating: (45) |
see fb H-status. also in forum: /tf/WW/en/Posts/28943 |
5/21/2012 3:52 PM | |
Posts: 14 Rating: (4) |
Hi rajudon, Attached to this post is a Step7-project. It contains 3 S7-programs. One of them is to fetch the status of all LED's in a H-CPU configuration (rack0 and rack1). Look at the status of the MSTR-leds on rack0 and rack1to determine wich one is Master at that moment. Good luck! Cheers, Tim AttachmentCPU_status.zip (669 Downloads) |
This contribution was helpful to2 thankful Users |
5/23/2012 4:53 PM | |
Joined: 7/2/2008 Last visit: 5/29/2024 Posts: 928 Rating: (306)
|
Hello rajudon, Please check, Best regards, H-H
|
Follow us on