(0)| 8/4/2012 11:35 AM | |
|
Posts: 1742 Rating:
|
Hello, I see an error code 0830 in the DB. In this manual: http://support.automation.siemens.com/WW/view/en/9260793, page 211, the error code is explained Extract: Master: A request message frame has been sent and the response monitoring time has elapsed without the start of a response message frame being detected. In other words, you did not get a response. Remedy from the manual: Check whether the transmission line has been interrupted (interface analysis may be necessary). Check that the same settings have been made on the module and communication partner for the following protocol parameters: transmission rate, number of data bits, parity and number of stop bits. Check that the value for the response monitoring time in PtP_PARAM is large enough. Check whether the specified slave address exists. The Modbus master system is only allowed to use the broadcast function for the function codes enabled for this purpose. |
| 5/26/2015 10:07 AM | |
|
Posts: 4757 Rating:
|
|
Follow us on