(0)| 9/1/2012 11:00 PM | |
|
Posts: 12 Rating:
|
Hello; Inmy project i am using a CPU313C (6ES7 313-5BG04-0AB0) and Simatic Manager V5.5 +SP2. When i want to test my program with physically I/Os iencountered a problem that i saw first time. Then i writed a simple program. I used smatic manager new project wizard. Select a CPU313Cwith default Hardware options. Default digital Inputs adressesare from 124 to 126 and default digital outputs adresses frop 124 to 125.. I write a simple program in OB1 as belown. Network 1 I124.0 Q124.0 ---| |--------------( )-- Network 2 I125.0 Q125.0 ---| |--------------( )-- Network 3 I126.0 Q125.5 ---| |--------------( )-- After download my program to CPU and run CPU. without any error. WhenI apply phsically digital 1 (24VDC)to I124.0 (i connect a push button to I124.0) Iviewed OB1online . I applied to I124.0 but i saw I126.0 =on and Q125.5 =on I did same thing with an other CPU313c, and i also tried with an other PC. Everytime i saw same thing. Network 3 I126.0 Q125.5 ---| |--------------( )-- What is the problem? I could not understand. I need your experiences. Please share with me. Regards. Attachmentcpu313.pdf (203 Downloads) |
| 9/2/2012 8:33 AM | |
|
Posts: 12 Rating:
|
Thank you Ayman Elotaify I did not notice before. This manuel explain all. First terminal X11 (on the left side) default input adresses start from 126.0. on X12 terminal's upside 124.0 and downside 125.0 Thanks for help. :) |
| 5/17/2017 12:11 PM | |
|
Posts: 4757 Rating:
|
New question published by OMKRIS2017 is split to a separate thread with the subject CPU integrated Inputs are not responding. Best regards |
Follow us on