(0)| 1/22/2013 8:39 AM | |
|
Posts: 15 Rating:
|
Hi All, I am using KTP600 Basic Color DP (6AV6 647-0AC11-3AX0) HMI. I am facing a problem related to the colour in alarms. I have selected use alarm class colours option and defined colours for activated, deactivated alarms etc. The problem is that, when it is downloaded to HMI the alarm texts are not showing the defined colours. The snapshots are also attached herewith. Kindly give suggestions. Regards, Meenu
AttachmentHMI- ALARM PROBLEM.pdf (234 Downloads) |
| 1/23/2013 1:11 PM | |
|
Posts: 3037 Rating:
|
Hello, Which version of WinCC flexibledo you use exactly? If you use the simulation on the pc, the problem appears also? Tweety |
| 1/24/2013 6:53 AM | |
|
Posts: 15 Rating:
|
Thanku for your reply..!! I am using WinCC Flexible 2008 SP3 Upd3. I am not using simulation from pc, using actual device KTP 600. Best Regards, Meenu
|
| 1/24/2013 12:02 PM | |
|
Posts: 3037 Rating:
|
Hello, Can you check your problem with simulation onyour PC? It is very interesting if the problem appears in the simulator also. Tweety |
| 6/19/2013 4:47 PM | |
|
Posts: 1 Rating:
|
In TIA Portal Click HMI> Runtime Settings>Alarms Then select "Alarm Class Colours"
|
Follow us on