(0)| 2/18/2013 6:03 AM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
Parallel connection of same type of power supplies for redundant operation More info at http://support.automation.siemens.com/WW/view/en/18123560 |
| 2/18/2013 6:42 AM | |
|
Posts: 7 Rating:
|
HiUMENCHO, Thanks for your reply. However, my question is not on the wiring or the whole setup itself, but rather the switch setting on the power supply. Should i use parellel operation at Switch A or single operation at Switch A. Refer document:BA_6EP1437-3BA10_7
AttachmentBA_6EP1437-3BA10_7.pdf (837 Downloads) |
| 2/18/2013 12:37 PM | |
|
Joined: 4/22/2010 Last visit: 3/31/2025 Posts: 5697 Rating:
|
Hello, This switch is used when you put 2 Sitop in paralel to increase performance. The output voltage regulation will be affected. For redundancy you need a powersupply that can power the installation by itself, the second supply is just in case 1 powersupply breaks, therefore diodes or a module is needed. Secure 24 V DC even when a power supply unit fails Regards, Marcjan |
|
Problem solved? |
|
| 2/19/2013 6:57 AM | |
|
Posts: 7 Rating:
|
HiMarcjan/UMENCHO, Thanks your explanation. I think i'm clear on the issue. Best Regards, Josh Cheang
|
This contribution was helpful to
|
|
| 1/15/2016 10:24 AM | |
|
Posts: 4757 Rating:
|
New question published by vikas soni is split to a separate thread with the subject Redundancy of two Siemens SITOP. Best regards |
Follow us on