9/2/2013 5:02 PM | |
Joined: 4/22/2010 Last visit: 3/31/2025 Posts: 5697 Rating:
|
Hello, Maybe if you mention the type of controller you have we could help you a bit. I suggest you also have a look at the Motoman site for more details of your controller and profibus communication. Motoman Netherlands did help me a lot with RS485 (not profibus) communication,try your local rep they might even have a Step7 example. Regards, Marcjan |
Problem solved? |
|
9/2/2013 7:49 PM | |
Joined: 9/27/2006 Last visit: 9/12/2025 Posts: 12407 Rating:
|
Hello avtel; Our friend Milosh found an easy solution for the integration of a new gsd file in TIA Portal: How to install GSD file on tia v11 The gsd file inserted in a S7-1200 PLC is used so the drive (or node of any kind) can be used as a Profibus-DP slave . However, a glance in the Yaskawa Motorman site shows that the available Profibus interface for the DX100 controller is as a remote I/O extension, the drive being a Profibus-DP master. What interface do you have on your DX100, and is it used as master or slave? Hope this helps, Daniel Chartier |
This contribution was helpful to
1 thankful Users |
4/17/2016 6:00 PM | |
Joined: 8/21/2014 Last visit: 9/10/2025 Posts: 1087 Rating:
|
New question published by support.automation.siemens.com is split to a separate thread with the subject Communication between Motoman robot (XRC controller, 2001) and S7-300. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on