(6)| 5/19/2018 11:34 AM | |
|
Joined: 3/14/2008 Last visit: 12/28/2025 Posts: 2233 Rating:
|
Hi dmitrii, the solution is in your post...you have Windows 10 Pro, but this OS is not released for PCS7. You need to have:Microsoft Windows 10 IoT Enterprise LTSB 2015 (64-Bit). |
|
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
|
|
| 5/19/2018 12:16 PM | |
|
Posts: 32 Rating:
|
Thank you! But I have Windows 10 Pro 64x. Not suitable? |
| 5/19/2018 2:07 PM | |
|
Joined: 3/14/2008 Last visit: 12/28/2025 Posts: 2233 Rating:
|
No, not suitable.. It is not released and thus not tested by Siemens. Also, you may have installed updates which could interfere with the install and use of PCS7. Maybe now you get the error because of it, I don't know. That is why only the 2015 LTSB version of Windows 10 is released. LTSB means that you not receive updates each week/month or so unlike regular Windows 10, so you won't have worry about updates screwing up PCS7. |
|
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
|
|
| 5/19/2018 4:16 PM | |
|
Joined: 9/9/2015 Last visit: 12/5/2025 Posts: 732 Rating:
|
Hi Dmitrii, Are you running for own engineering development or for customer? If for your own development station, you could run your software using VMware? run with vmware player, install window 7, install pcs 7. Then you do not need to worry about the compatibility anymore. Hope it helps. |
|
Please give me 5 stars Rating if my post is helpful for you. :) |
|
| 5/21/2018 8:01 AM | |
|
Posts: 32 Rating:
|
Oreca, Thank you very much! |
Last edited by: dmitrii.anyushin at: 5/21/2018 8:02:04 AM |
|
| 5/21/2018 8:03 AM | |
|
Posts: 32 Rating:
|
JazTai. No, I work for a client and VM does not suit me |
| 5/21/2018 6:15 PM | |
|
Joined: 3/14/2008 Last visit: 12/28/2025 Posts: 2233 Rating:
|
It could be this version is not available for download anymore. I know you can order a IPC pre installed where the ltsb 2015 is supplied, maybe Siemens can deliver the LTSB 2015? Maybe I have it, so I can upload it for you, but you need to buy a license. |
|
If I could help you, you can use the RATE button. Thank you. |
|
| 8/30/2023 7:21 AM | |
|
Joined: 9/9/2015 Last visit: 12/5/2025 Posts: 732 Rating:
|
This solution is working. I created another post with more details on PCS 7 V9.1 SP2 / WinCC V7.5 SP2. |
|
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to
|
|
| 9/19/2024 1:53 PM | |
|
Joined: 9/19/2024 Last visit: 8/19/2025 Posts: 3 Rating:
|
Hello I installed Windows 10 enterprise LTSC 2018 but I have this problem. |
Follow us on