(3)| 6/30/2015 5:20 PM | |
|
Joined: 8/31/2005 Last visit: 12/16/2025 Posts: 2198 Rating:
|
Use the slice access or: Define a PLC-Data-Type for your scanner (including all 32 Bytes) and define/name your OI with it. Then you can uses the individual signals in your program. I added screenshots, where I used it for a drive. Note there are 16 bits and one INT in the PLC data type defined. In your program you can use the symbol browser to get the possible signals. (The 16 bits are shown when a BOOL has to be selected and the INT if you need a INT) Attachmentscreenshots.zip (1282 Downloads) |
Last edited by: miami at: 6/30/2015 5:21:22 PM |
|
Follow us on