(7)| 4/28/2016 2:44 PM | |
|
Joined: 5/28/2008 Last visit: 12/29/2025 Posts: 4522 Rating:
|
Hello, Please read these useful links: What is the difference between Ethernet and Industrial Ethernet? |
|
Ayman Elotaify |
|
This contribution was helpful to
|
|
| 4/28/2016 2:49 PM | |
|
Joined: 9/27/2006 Last visit: 12/30/2025 Posts: 12479 Rating:
|
Hello HVK; There are many sources of information on Profinet available, both on this site and on the web; search for more threads on the same subject as yours. One of the best sources is Profibus.com, developed and maintained by Profibus International. For example, this document should provide information you would appreciate: http://www.profibus.com/nc/download/technical-descriptions-books/downloads/profinet-technology-and-application-system-description/display/In this technical document (as in most technical information you can find on the subject) they refer to Ethernet as IEEE 802, which is a series of standards that define the requirements (physical and protocols) for the implementation of LANs and WANs. If you are interested in the basis of Ethernet standards, look at this presentation: The document I proposed at the beginning (Profinet system description) shows a graph explaining the relationship between Ethernet and Profinet: look at the very bottom of the diagram, way down, you will find the IEEE 802 standards as a base for development of Profinet standards, protocols and application profiles. In OSI model terms, Profinet follows and applies the Ethernet physical layer and data link and transport layers. which means that other Ethernet-based protocols (Modbus/TCP, Ethernet/IP, FTP...) can co-exist with Profinet on the network, which uses Ethernet structured cabling and switches and TCP/IP adressing. Then specific protocols and profiles for Profinet are added and integrated to make Profinet distinct from other applications. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 4/28/2016 3:27:05 PM |
|
This contribution was helpful to
|
|
| 4/28/2016 5:45 PM | |
|
Joined: 3/28/2015 Last visit: 12/29/2025 Posts: 727 Rating:
|
Hello, Kindly find the attached file. AttachmentProfinet_Ethernet.pdf (1679 Downloads) |
|
Eng.Mohamed Ibrahim |
|
This contribution was helpful to
|
|
| 4/29/2016 9:40 AM | |
|
Posts: 42 Rating:
|
Dear All, Thanks for Reply.. Now I can Realize the difference between Ethernet And Profinet . |
This contribution was helpful to
|
|
Follow us on