(1)| 9/19/2016 1:12 PM | |
|
Joined: 5/12/2006 Last visit: 12/19/2025 Posts: 22816 Rating:
|
Hi, why a new Thread the problem always disscused here: If you use the integrated routing you should not use the device Acces, you must use the S7ONLINE access, then the Routing adresses are filled out from the system automatic. If you use the Device you must insert all relevant information:
Christoph |
| 9/19/2016 1:55 PM | |
|
Posts: 179 Rating:
|
Christoph, CPU 315-2PN/DP 25 of the Sinamics are version 3.x and new one is 4.6 I attached a print screen of the FW displayed in accessible Nodes are just Ethernet addresses not Profibus, I couldn't get any Profibus addresses (on normal PC with starter connected to Profibus cable I can see all Nodes but by this Field PG M4 just Ethernet addresses displayed because of Field PG/PC comm setting to TCP/IP). And error window is on the previous print screen. if something missing I can add. Sorry if I am not as clever as others to find the problem by myself. Thank YOU
AttachmentFW.zip (631 Downloads) |
Last edited by: AhooraJafari at: 9/19/2016 2:41:29 PMLast edited by: AhooraJafari at: 9/19/2016 2:46:41 PM |
|
| 9/19/2016 3:47 PM | |
|
Joined: 5/12/2006 Last visit: 12/19/2025 Posts: 22816 Rating:
|
Hi, ok is your decision. Regards |
Follow us on