3/23/2021 8:59 AM | |
Joined: 9/9/2015 Last visit: 4/9/2025 Posts: 732 Rating:
|
Hi All, I would like to share a weird experience i have on this " No Connection To Data Server "Topic. Case Study 1. The system is PCS 7 V8.0 Up1, Windows Server 2003. 2. Both OS Servers (Master and standby) was running good. 3. OS_B runtime deactivated manually, but unable to complete deactivation. 4. Used reset_wincc to kill the process and do something. 5. restart and try start up, OS project is not responding , stuck at Autostart. Project cannot be opened. 6. restart the system and cancel the autostart. Download OS Project WinCCAppl_Stby from ES. Executed successfully. 7. restart OS_B. Autostart successfully. But when the OS_B activated and go into runtime, alarm one line showed "No Connection to Data Server" . 8. after 30 seconds , force restart windows popped out , " An error has occurred that requires a restart of computer" (seem like a simatic net issue) 9. After checking around, Terminal Bus adapter was disabled. 10. Restarted and check the Ping, simatic shell, station configuration , the result are all the same. No connection to data server. 11. Since the OS_A is running and the production cannot be stopped, i have no choice but to continue at next available chance. 12. I shutdown the OS_B station for a night, and restart the second day. 13. OS_B booted into runtime without issue. Weird experiences. At the end, my solution is, download the OS project again, and "SHUTDOWN" , then start it again. Hope it is helpful for someone in the future. For other related topics, please refer below: 1. No Connection to data server - 20200811 2. No connection to data server - 20171201 3. WinCC Alarm Logging - 20140820 4. No Connection to data server - 20140827 5. No Connection to data server - 20150907 |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to
2 thankful Users |
Follow us on