5/29/2012 10:37 PM | |
Joined: 2/16/2011 Last visit: 4/28/2025 Posts: 229 Rating:
|
Hello, I start to convert the library... Regards
AttachmentOSCAT_V11.zip (4041 Downloads) |
Last edited by: Gabriel de Oliveira at: 7/9/2012 10:29 PMIncluded the *.al11 file Gabriel de Oliveira |
|
This contribution was helpful to
7 thankful Users |
5/30/2012 4:23 PM | |
Joined: 2/16/2011 Last visit: 4/28/2025 Posts: 229 Rating:
|
Huggy, Here is all the source exported files from Step7 v5.x. Now you can import to your TIA Portal and study the codes I'm Learning a lot. I thinking to create a new post or Tip for this subject. Regards
AttachmentOSCAT Exported SCL Files.zip (3282 Downloads) |
Gabriel de Oliveira |
|
This contribution was helpful to
1 thankful Users |
7/6/2012 9:09 PM | |
Joined: 9/24/2009 Last visit: 9/17/2025 Posts: 2 Rating:
|
Helo, Gabriel. In your attachment OSCAT_V11.zip missing file OSCAT_V11.al11 and I can't open library
|
7/9/2012 10:30 PM | |
Joined: 2/16/2011 Last visit: 4/28/2025 Posts: 229 Rating:
|
Dear App$, Problem solved.
|
Gabriel de Oliveira |
|
10/2/2012 7:30 PM | |
Joined: 7/7/2010 Last visit: 9/17/2025 Posts: 16112 Rating:
|
Today Siemens released an SCL Conversion tool (Deutsch/English language only) for free download. It batch converted the entire OSCAT SCL library uploaded in this thread. I zipped up the entire folder (attached). Some things will not work no matter what you do because of the significant differences between S7-300/400 & S7-1200. However, this conversion seems to fix lots of the problems encountered during the conversion, some of which I had not run across with this library of open source logic. It is a big package that unfortunately cannot simply be compiled into a single library and then be used as is - there are duplicate scl source files in multiple directory locations, but each folder can be a self-contained library. AttachmentOSCAT_After_SCL_Converter_ForTIAPortal_V1x.zip (1877 Downloads) |
science guy |
|
This contribution was helpful to
7 thankful Users |
8/6/2014 1:01 PM | |
Joined: 2/16/2011 Last visit: 4/28/2025 Posts: 229 Rating:
|
DearGaJEnDrA.D.S, Huggy has posted an updated version. Try that!
|
Gabriel de Oliveira |
|
This contribution was helpful to
1 thankful Users |
1/8/2018 11:32 AM | |
Joined: 2/9/2016 Last visit: 7/7/2024 Posts: 3 Rating:
|
Thanks for this. I was also porting some of the most interesting scl-fragments to 14, but this is very good. |
Follow us on