(0)| 3/8/2022 10:56 AM | |
|
Posts: 8 Rating:
|
Hi cookie 🤗, thank you for replying the WinCC version is V7.0 + SP3 + Upd1 the OS version is windows server 2008 |
| 3/8/2022 12:04 PM | |
|
Joined: 10/16/2020 Last visit: 1/14/2026 Posts: 146 Rating:
|
Hi, There are several versions of Windows Server 2008. Make sure of compatibility with the Kompatool. On the other hand, you can try to install the latest available update for your WinCC. Cookie_M0nster. |
|
If this information has been helpful to you, please don't forget to rate it. |
|
| 3/8/2022 1:45 PM | |
|
Joined: 8/3/2009 Last visit: 1/20/2026 Posts: 16653 Rating:
|
Hello M.badawy Do I understand correctly that you do not get connection from the WInCC Client to the Server? Then check first this FAQ on all PCs: https://support.industry.siemens.com/cs/de/en/view/868014 then Check the general Information in this FAQ: https://support.industry.siemens.com/cs/de/en/view/109771695 Then everything should work. It could be a reason of name resolution, rights or SIAMTIC Shell settings. Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
| 3/10/2022 11:15 AM | |
|
Posts: 8 Rating:
|
Hi Murof, I will drag photos to my issue |
| 3/18/2022 6:37 PM | |
|
Posts: 8 Rating:
|
Hello murof, I checked the s7 protocol suite and also I checked pg/pc setting and selected the correct TCPIP but the problem doesn’t solve |
Follow us on