2/6/2015 7:31 AM | |
Posts: 1 Rating: (0) |
Hi, This is very helpful thanks but i need more details my project is to use CPU 1212c DC/DC/DC and 2 pulse encoder 100PPR the cpu with the aid of analog o/p to drive dc 'SPRINT DRIVE' what i need is analog signal Acceleration Referance Speed Deceleration with the encoder feed back the speed never excced 400mm/s how to configur PID to give the analog ----------------- Splitted from motion control. |
Last edited by: Min_Moderator at: 2/6/2015 2:54:05 PMNew subject after splitting |
|
Follow us on