9/16/2012 4:41 AM | |
Joined: 7/8/2009 Last visit: 8/5/2024 Posts: 1976 Rating:
|
Well, This is not Auto Reset problem so dont go for it Now, i have seen same things in few cases. Things to check - P640- Your current Limit, r0027 Actual current What control mode is selected? If it is V/F ( P1300=0), try to go for SLVC (P1300=20) For this, you need to do optimization also to get good result (P1910 & P1960) Refere Manuals - Operating Instruction and Parameter List Regards, Devesh Vithani |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
5/9/2017 1:10 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4769 Rating:
|
New question published by AutoGen_440202 is split to a separate thread with the subject Simadyn D, when drive started with load it was dispalaying alarm. Best regards |
Follow us on