2/13/2017 9:46 AM | |
Posts: 10 Rating: (0) |
Hallo, Thank you for reply. the Program itself doesn't contain so much code...I just call one FB in OB35 and write to output. I've put OB35 as PIP1 and DO card of this Output is also in PIP1 - rest of DO cards is OB PIP. The output in Monitor mode of DO card does come as true in HW config, but no Output to Card. But , I've been use Monitor/Modify from HW config and none of outputs wont to be written - in HW config/Monitor - they are green, on the card nothing. I think that PIP settings for the card should not be important for HW Monitor/modify...Most strange is that when I connect the Et200m to the S73152DP - Digital outputs are written normally. Its really confusing situation. If you think I can send you some more information - let me know. Thanks for your support AttachmentCPUSettings.zip (306 Downloads) |
2/13/2017 1:31 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by Faizan Taufiq is split to a separate thread with the subject S7-400 not communicate and generate BUS1F. Best regards |
Follow us on