12/3/2018 9:34 AM | |
Posts: 25 Rating: (0) |
Hi I want to know the following : [snip] 2-Is S7-1517h for non-critical application only [snip] thanks ------------------------------------------------------------------------------------------ ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/3/2018 2:49:40 PMNew subject after splitting Last edited by: Jen_Moderator at: 01/31/2020 13:56:28New subject after splitting. Division of questions into separate topics. |
|
12/5/2018 11:51 AM | |
Joined: 7/2/2008 Last visit: 9/30/2024 Posts: 928 Rating: (309) |
Hello Hussein, Yet, there are no much information on S7-1500H. Even the conference tag is still S7-1500. I will try to answer according to answers I already have from Siemens and also according to my experience with H systems compared to what I read in S7-1500H manual.
1&2 - As per Siemens guys' statements in SPS fair last week, the S7-1500 is mainly targeting discrete automation and it's not even for safety/critical applications in discrete automation. No Safety in S7-1500H. S7-1500H is not to replace S7-400H. The redundant controllers for process industry are the ones of 400H controllers which will be still available beyond 2030. [snip] Best regards, H-H |
Last edited by: Jen_Moderator at: 01/31/2020 14:02:06Division of answers into separate topics. |
|
This contribution was helpful to1 thankful Users |
1/31/2020 1:54 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by husseinwaledia is split to a separate thread with the subject Is s7-400h is better than 1517h?. Best regards |
Follow us on