6/6/2016 10:24 PM | |
Posts: 5225 Rating: (1192) |
Hi. <Murof> has given good ideas. I thought I would follow it through to make some sort of instructions. Attached is a sample program, picture notes on what to look for in the program and also a PDF on step-by-step how to use the simulation of the example program. The example has 2 pages. If you log in on page 1, the next page will open. If the user allows the log-in to expire, the system automatically go back to page 1. To refresh the log in time-out, you will have to have tasks that is password protected. This should be on page 2 of the example and is currently not there. There is an easier way to achieve what you ask. Simply add password protection to every task. The user can only use the task if he is logged on. This is also explained in the notes on how to do that. I am curious to hear your feedback on how these notes can be improved and if it is helpful to you. Best of luck. AttachmentKTP300 password example.zip (255 Downloads) |
Last edited by: William_B at: 6/6/2016 10:34:59 PMNOTE: "KTP300" is a typing error.... it should be "KP300" |
|
This contribution was helpful to1 thankful Users |
6/7/2016 11:10 PM | |
Posts: 200 Rating: (6) |
Hi i have added all the elements into the program and seem to hit a problem that is quite strange. when i run the program in simulator its perfect. when i down load to the screen the password is in valid. any ideas AttachmentMESSAGES_V3.zip (134 Downloads) |
6/8/2016 10:08 PM | |
Posts: 5225 Rating: (1192) |
Hi Andrew,
Nice!!
Ouch! Regards. |
6/9/2016 8:15 PM | |
Posts: 200 Rating: (6) |
Hi Sorry the wrong folder this is the latest i like the idea of being able to do the following of a admin and user i would like the user to be able to use F1 and F2 but not F8,F9 and F10. will look into this but if you point me in the right way thanks andrew AttachmentMESSAGES_V4.zip (167 Downloads) |
Last edited by: andrewdaw1978 at: 6/9/2016 9:23:03 PM |
|
Follow us on