1/26/2016 1:52 PM | |
Posts: 1 Rating: (0) |
This is from manual on this module 6ES7 138-4DA04-0AB0 : "Connectable Counting Signals The 1Count24V can count the signals of the following encoders: ● 24 V pulse encoder with direction level ● 24 V pulse encoder without direction level ● 24 V incremental encoder with two tracks that are 90o out of phase (rotary encoder)."
How can I connect this encoder and module to see the signal? I have read manual but don`t understand how i can do it. |
Last edited by: Zhyleo at: 1/26/2016 2:25:37 PMLast edited by: Zhyleo at: 1/26/2016 2:51:25 PMLast edited by: Zhyleo at: 1/26/2016 2:52:19 PMLast edited by: Zhyleo at: 1/26/2016 4:12:42 PM |
|
9/14/2023 8:36 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by candemirhalil is split to a separate thread with the subject S7-1200 and ET200: How is ladder writting ? . Best regards |
Follow us on