5/14/2020 6:56 PM | |
Joined: 4/15/2020 Last visit: 9/4/2023 Posts: 7 Rating:
|
Hi, just some info on the things I've experienced the last days playing with the example image for the iot 2050. First, using Linux Mint, I have no problem building the example image as explained on github.com/siemens/meta-iot2050. However once the image is copied to a sd card or usb stick, I'm only able to let it boot 1 time. Once I press the reset button, powercycle or restart the system, the image doesn't boot anymore. I've connected a monitor to the displayport and the only thing that I see is 2 Linux Tux's and a blinking cursor. The first time I've boot the system, after a while a normal login prompt appears, but now after restarting this doesn't happen anymore. Result an incomplete boot. I realized that the kernel boot log, is not displayed on my monitor, so I've connected a ftdi TTL to usb adapter to the debug port. Now i can see the complete bootlog. (see attachement) As you can see the booting stops once the kernel tries to load the rootfs. Waiting for root device PARTUUID=20c5e49d-f8f5-4e3c-9427-7379c6a97962... The quickest way to create a workaround for this is to create a new boot/boot.scr file. howto: copy the "boot.scr" content, minus the weird characters at the beginning of the file, to "boot.txt". edit boot.txt with root=/dev/sda1 create a new boot.scr using the following command mkimage -A arm -O linux -T script -C none -n "My Boot" -d boot.txt boot.scr mkimage is part of the u-boot-tools package (Debian) I hope this is helpful for people experiencing the same problem regards, Kris Attachmentbootlog.txt (699 Downloads) |
5/15/2020 3:49 PM | |
Joined: 4/28/2015 Last visit: 6/28/2024 Posts: 578 Rating:
|
Oh, and your workaround can be achieved even easier:
|
Follow us on