2/5/2017 1:22 PM | |
Posts: 13 Rating:
|
Hi every body, I am very new to siemens platform. My previous experience with Allen Bradley. I wanted to know how to communicate with S7-200 over siemens PG. How to set communication. Thanks in advance. Regards, ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 2/6/2017 3:53:33 PMNew subject after splitting |
|
2/12/2017 11:07 AM | |
Joined: 4/28/2015 Last visit: 4/19/2025 Posts: 10876 Rating:
|
Hello, ok, I see some missunderstanding but no problem. As I sugested before, if you have PG M4 you have CP5711 integrated so you don't need use any other PPI cable/adapter. Only connect your PG with S7-200 via classic DP cable fitted with DP connectors. As I have also PG M4, it is delivered with original cable for connection, but I recommend use that DP cable. In case of not existing option in PG/PC inreface about MicroWin, try use that attached bat file, but for first close all Siemens SW instances for sure, also that PG/PC interface. Look for first what is inside, check that path existing, you can also go directly manually and run that exe with - up parameter manually. Leave that bat file run to end, it can takes some time. After all it can automatically disappear. After that you can have hope that MicroWin option available in PG/PC inteface. Give us other infos and good luck. Update: mybe also important question, what version of MicroWin do you have installed? Only v4.0 SP9 is compatible with Win7 versions. Update2: aaaah now I see that you've change picture to better visible. As I see you have select CP5711, this is correct but if you don't have right available access point, no luck. Try my sugestion. AttachmentSimatic_PGPC_Update.zip (1047 Downloads) |
Last edited by: Duris_I at: 2/12/2017 11:11:29 AMLast edited by: Duris_I at: 2/12/2017 11:11:50 AMLast edited by: Duris_I at: 2/12/2017 11:38:45 AMWith best regards... |
|
This contribution was helpful to
1 thankful Users |
2/13/2017 1:58 PM | |
Joined: 4/28/2015 Last visit: 4/19/2025 Posts: 10876 Rating:
|
Hello, good news, you're welcome. Good luck. |
With best regards... |
|
Follow us on