7/17/2017 6:30 PM | |
Joined: 12/2/2008 Last visit: 10/14/2024 Posts: 107 Rating: (2) |
Hello Denilson. Do you know if It can be used on a S7-1200 CPU?. Currently I am trying on it but I get Errors when I try to read the Memory Area. InOut Point_Array Array[*] of Bool Salida Bool Temp Start DInt End DInt i Int #Start := LOWER_BOUND(ARR := #Point_Array, DIM := 1); #End := UPPER_BOUND(ARR := #Point_Array, DIM := 1); #i := 0; FOR #i := #Start TO #End DO IF #Point_Array[#i] THEN #Salida := TRUE; RETURN; END_IF; END_FOR; #Salida := FALSE; Thank you Regard. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/25/2017 8:24:12 AMNew subject after splitting |
|
7/25/2017 8:25 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice.
|
Follow us on