(0)| 3/14/2018 8:45 PM | |
|
Posts: 2 Rating:
|
In my case, I need to migrate Panel PC 677 to IPC677D. 6AV7804-0BB12-0AC0 to 6AV7260-1DG10-0AX0. The RunTime will be compatible? Because the first is WinXP and other is Win7Ult 32.
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/15/2018 2:28:44 PMNew subject after splitting |
|
| 3/27/2018 2:50 PM | |
|
Joined: 10/18/2012 Last visit: 12/1/2025 Posts: 225 Rating:
|
Hello Eduardo, an IPC677D can run with different Operating Systems:
It depend's on the Software, that should run on that IPC, to determine which operating system will fit best. Not every Software can run on every operating system. A lot of Siemens Software packages are tested with different operating systems. The results are stored in a database inside the compatibility tool at www.siemens.com/kompatool. In step 1 just select your Softwareproduct as Main-Product, e.g. WinCC V7.3 and then continue to the next step. If you prefer Microsoft Excel sheets, this is also possible. Some notes about WinCC: Otherwise you have to re-engineer the project, which can result in a significant effort! best regards, |
Last edited by: xnor at: 3/27/2018 2:54:51 PMadded Windows 10 LTSB 2015 |
|
Follow us on