11/11/2019 9:15 AM | |
Posts: 1 Rating: (0) |
Dear Experts, I'm Working on resolving one downloading issue to AS AS: 414-4h ES: PCS7 V7 OS: WinCC Redundant Server I am using cp443-1 v1. when I want to configure the hardware, PN IO,X1 and X2 get addresses(port) automatically. it seems ok but after download cpu go to stop. i try that on PCS7 v8 but the ports does not get addresses anymore. it's marvelous. tell me what can I do. note: i have to use PSC7 V7 cp443-1 order is 1ex20-0xe0 v1 the errors on the diagnostic buffer are like that: parameter assignment error preventing startup in address parameters for submodule Parameter : slot input address :8177 error type: illegal parameter coding ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/11/2019 10:59:11New subject after splitting |
|
Follow us on