(0)| 2/2/2009 12:23 PM | |
|
Posts: 25 Rating:
|
Hello, Delete all your temporary files from the options menu, and do re-build all in the file menu. Hope this work. Thanks & Regards, Thavas |
| 7/27/2009 12:27 PM | |
|
Posts: 1 Rating:
|
Hello I have these same problem in WinCC 2008 and deleting temporary files and rebuilding project doesn't help. |
| 7/27/2009 2:05 PM | |
|
Joined: 5/8/2006 Last visit: 10/23/2025 Posts: 1085 Rating:
|
Hi Did you see the second device in the transfer dialog? Maybe you can deselect the second HMI device. Ifthe second device isnot available, then it seems thatthe data base is corrupt of the project. Maybe the development of WinCC flexible can repair your project. You shouldcreate an Service Request at the hotline. Alternative you can use your both original projects and try the second possibility which is describedin the following link: http://support.automation.siemens.com/WW/view/en/23844410 Bye |
Follow us on