(0)| 3/3/2012 2:15 AM | |
|
Joined: 10/7/2005 Last visit: 1/20/2026 Posts: 3054 Rating:
|
Hello Bjekas I'm afraid to say that 2048 Bytes is theupperlimit of retentive data in a 1200 and below is an excerpt from the S7-1200 manual (ref. chapter 4.1.6): "A total of 2048 bytes of data can be retentive. To see how much is available, from the PLC tag table or the assignment list, click on the "Retain" toolbar icon. Although this is where the retentive range is specified for M memory, the second row indicates the total remaining memory available for M and DB combined. Note that for this value to be accurate, you must compile all data blocks with retentive tags." Possibly not the answer you wanted to hear, but I hope it helps anyhow. |
|
Cheers |
|
Follow us on