(3)| 3/10/2014 6:46 PM | |
|
Posts: 8946 Rating:
|
What you tell us is wrong. Please check again the speed values. |
| 3/10/2014 7:52 PM | |
|
Posts: 8946 Rating:
|
Some MPI Interfaces can do 12 Mb/s, but 13,2 is not possible. |
| 3/10/2014 10:05 PM | |
|
Posts: 133 Rating:
|
What I found is that the transmission speed of an RS485 can reach 12 MBauds, and given that RS485 is a physical support for MPI as well as Profibus, I concluded that MPI can reach 12MBauds. |
| 3/10/2014 10:13 PM | |
|
Posts: 133 Rating:
|
I found, from a SIEMENS document, that the CPU IM151-7 transmission speed is "exactly" 12 Mbps, which is equivalent to 13,2 MBauds. |
| 3/11/2014 8:40 PM | |
|
Posts: 8946 Rating:
|
|
| 3/11/2014 11:44 PM | |
|
Posts: 133 Rating:
|
hey!! If I'm wrong, what are you waiting to tell me the correct equivalent? |
| 3/12/2014 12:39 AM | |
|
Joined: 10/7/2005 Last visit: 12/29/2025 Posts: 3052 Rating:
|
Hello allayahassine let me start byclaimingthat you as well as our friendIBN-Serviceare both correct, albeitIBN Service isabsolutely correct. You are generally correct that the terms bpsmustnot be confused with theterm baud. Whereas bps isthe number ofbits per second, baud is number of symbols per second and these two values can differ (commonly found when moduation based transmissions are used where a symbol can contain multiple encoded bits so you can for example have 1200 baud but an effective bitrate of 4800 bps). Profibus DP is though NRZ (Non return to Zero) encoded, so a bit represents a symbol (and vice versa) which means that bps is the same as baud. The same applies forMPI which is Siemens proprietary subset of Profibus DP (butuses the same physical Layer). In sums: 12 Mbps = 12 Mbaud in case of Profibus DP and MPI and I hope this helps |
Last edited by: fritz at: 3/12/2014 5:51 AMtypos Cheers |
|
This contribution was helpful to
|
|
| 3/12/2014 8:39 AM | |
|
Posts: 133 Rating:
|
thanks |
Follow us on