4/7/2014 6:09 PM | |
Joined: 7/15/2009 Last visit: 7/31/2024 Posts: 30 Rating: (0) |
it's ok , i have diffrent problem , i made the connection with the plc and see it very well , and can be online but when i start to make the second important step which is ( upload the program in the cpu with the same ID CPU214c dc/dc/rly to my pc ) . i get this message(attached) , can any expert help me to know what is the problem ???????
Attachmentcan't upload.pdf (268 Downloads) |
Last edited by: CS Moderator at: 4/8/2014 11:47 PMnew subject after splitting from /tf/WW/en/Posts/91058#top Last edited by: abosama at: 4/7/2014 7:07 PM |
|
5/31/2016 2:05 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by samuel1707 is split to a separate thread with the subject TIA V13, while upload, error that system is unable to detect the hardware. Best regards |
Follow us on