Industry Online Support
Technical Forum
4/7/2014 7:08 AM | |
Joined: 8/5/2010 Last visit: 4/5/2024 Posts: 27 Rating:
|
Dear Experts, Any idea/solution for the above problem |
4/24/2014 9:38 AM | |
Posts: 220 Rating:
|
Do you try to download just the chages? Maybe is the download of the hole project the reson why you lost the archive data.
|
9/12/2014 10:04 AM | |
Posts: 567 Rating:
|
hi pash, did you have taken your OS project online on ES? In PCS 7 it is not useful to start OS runtime on ES For testing your OS project you can use the OS simulation function on ES! If yes, youshould do the steps which are described in FAQ "What should you do if the OS server project is taken online by mistake on the ES?". Link to FAQ: http://support.automation.siemens.com/WW/view/en/24285161 |
Follow us on