5/9/2014 2:11 PM | |
Joined: 1/28/2012 Last visit: 9/15/2023 Posts: 519 Rating: (83) |
Can you attach screenshot of error? What exact error is occured? |
Regards, |
|
5/9/2014 8:49 PM | |
Joined: 10/3/2010 Last visit: 4/29/2024 Posts: 1552 Rating: (188) |
[quote user="nnkrish19"]Dear firends, I am Facing problem in Wincc 7.0.3. Whenever power cut occurs while wincc Runtime was in Active, We facing problem to open Application Program. Even we tried by reinstalling Wincc. But we cant solve the problem. I need to format, New OS installation the Wincc installation has to done then and then only Wincc communiating with PLC. I faced this problem many times. Kindly give some suggestion for above issue. Thanks in advance.
Power cuts many times? I think you should solve that problem as that's the source of your problems. Not only WinCC can be damaged or your OS by power cuts but also your hardware.
If you can't solve power cuts for some reason, you should really consider a UPS.
|
B r g d s , |
|
5/9/2014 9:37 PM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (270) |
Hi, There are couple of things needs to be addressed. One thing you didn't mention reagrding UPS availablity. 1) you need to ensure that there is no freqent power failure. 2)Are you using an UPS? 3)When yourWincc get crashed while Power Cut, Please check event log files for error. if possible please attach here. 4)have you installed latest Hotfix for Wincc 7.0.3? Update 6 for WinCC V7.0 SP3 und WinCC V7.0 SP3 ASIA Also, There is an addon product called Shutdown WinCC is available. See the following link: 1) Shutdown WinCC Following FAQ might help you. 2) How do you safely terminate WinCC by means of an external application? |
Last edited by: Amit_86 at: 5/9/2014 9:39 PMVANDE MATARAM..... |
|
This contribution was helpful to4 thankful Users |
5/19/2014 7:57 AM | |
Joined: 10/3/2010 Last visit: 4/29/2024 Posts: 1552 Rating: (188) |
Hey Abdalkade, thx for explaining, I'm sure this is a workable solution for you and probably timesaving but if WinCC gets corrupt often, I would recommend to find the real cause. WinCC shouldn't get corrupt often. |
B r g d s , |
|
Follow us on