(0)| 7/26/2007 2:56 PM | |
|
Posts: 7 Rating:
|
Dear TechTeam We are using a lot of quantity master drive-mc dc/ac (6SE7012-OPT50-Z)Z=F01+G91+C23+G42. Slot A-CBP Slot B-SLB Slot C-SBR1 with motor (PARKE S.B.C model # SMB 823003814S5R64) with simatic S7-300 through frofibus.I want to run it independently in our Lab. for checking purpose only.My question is, can I run this inverter and motor in our Lab through X101, with out S7-300.if yes then 1-What will be the parameters and wiring diagram? 2-can we use normal 4 pole motor on it for checking purpose only in speed control mode. Can you provide schematic diagram of this drive, so we repair all drive easily in our lab.I am sending you parameter file which we are using presently.Please help me. Thanks in advance. Rand Attachment: masterdrive.zip |
Last edited by: Rand at: 5/28/2008 7:37 AMLast edited by: Rand at: 5/28/2008 7:32 AMLast edited by: randhawa at: 31.07.2007 07:13Last edited by: randhawa at: 31.07.2007 07:06 |
|
Follow us on