(0)| 5/22/2014 3:28 PM | |
|
Joined: 1/5/2011 Last visit: 3/13/2025 Posts: 815 Rating:
|
Ok, let me clarify the first two answers with a screenshot (check attachment). Q/A Q:
A:
More info 1)Ok so the first screenshot shows your alarmview can view the whole alarmdatalog if you enable that option. What is viewed and logged can be defined by the user. (warning, alarms, system events,...). 2)The second example shows that you are able to create your own "event", if everything is configured right, you can logthat event and display it on the alarmview. The script is just an example,you will have to "pimpthe script"to your requirements. I will explain what the script is doing in my case,ifan ADD button is pressed the script is executed. When an eventtext is insered that eventtext will be show as systemalarm and added to the log. Now if you can change the script to your needs and for example log your eventtext if the user changes (scheduled tasks), etc..
3)Check out this link: Printing with SIMATIC Comfort Panels Here you can download a sample program, you can add your alarmview to a report window and then print that report, it might solve your problem... Please confirm if you've been able to print your datalog viareports. Hope this helped. Kind regards, Jens |
Last edited by: Jens_app at: 5/22/2014 3:48 PMLast edited by: Jens_app at: 5/22/2014 3:33 PMKeep it simple and on-topic. |
|
| 5/23/2014 12:03 PM | |
|
Posts: 7 Rating:
|
Thanks a lot sir. I tested it and it works. There is still another problem. I need to have this printout. (See attachment). There is some tags value and label to be write on the text.files before the datalog start. Is the HMI capable to print this format? Do i need to script? I worry if the HMI is capable to print with the format in the attachment. Thank you.
AttachmentTemp Logging.pdf (707 Downloads) |
| 5/23/2014 12:24 PM | |
|
Joined: 1/5/2011 Last visit: 3/13/2025 Posts: 815 Rating:
|
Hello jdpapa, as I described before, you can create a VBS script to achieve what you want. Check my previous posts, I attached a file there: attachment: Logviewandadd.jpg (5 Downloads)I've also attached a new screenshot(which is more clear)to show you how it can be done. You will see by using ShowSystemAlarm("Tag") in your script, you can addtext to your log (and your alarm view). For example if PLCTAG = Jens and you use in your script:ShowSystemAlarm "OperatorName:" & SmartTags("PLCTAG")in your alarmview (and log if settings are done correct) there will appear"OperatorName: Jens". Hope this solved your problem. Kind regards, Jens |
|
Keep it simple and on-topic. |
|
Follow us on