(0)| 6/12/2014 5:23 PM | |
|
Posts: 7298 Rating:
|
Hello, if your are missing the pixel size 1600x900 in the available layouts, you can modify the configuration file, itis in the installation path of WinCC. The complete path depends on the resolution and project type. It has the following structure: "...\SIMATIC\WINCC\options\pdl\SIMATIC_<Screen resolution> <Project type>\SIMATIC_<Screen resolution><Project type>.cfg" see: http://support.automation.siemens.com/WW/view/en/27037661 Regards Georg |
| 6/17/2014 4:19 AM | |
|
Posts: 107 Rating:
|
thank you bg2492... before I couldn't open the cfn file now I'm gonna do it regards IT_Service
|
Follow us on