(0)| 6/17/2014 10:47 AM | |
|
Posts: 206 Rating:
|
Hello Rajnish, As I understood you have weigh deviation if "odd" weight are on the scale?? If there are even weight on the scale you have no deviation?? What send option, that get diabled,you mean? May be you open a support request http://support.automation.siemens.com/WW/view/en/16605654and attach the following information's: - no., nominal load and type of the used load cells - dead load (e.g. hopper) of the scale - PLC program with infomation's where you use the Siwarex module - procedure how you try to calibrate - a table where you show the applied weight and the weight is shown by the Siwarex U - some photos of the scale and the mounted load cells With these information's it might be possible to help you. Regards ABenno |
Follow us on