(1)| 7/3/2014 3:46 PM | |
|
Posts: 4620 Rating:
|
Hello JKTUNG, As for the CPU 22x I think that there are no problems, but with the CPU 21x I think it is not possible to put the EM277 because they are older CPUs, if you look at the manual on page 9-15 speaks of the CPU 215 that the integrate interface for Profibus, so I do not think it's possible. System Manual S7-200 Programmable Controller - Siemens Document for 6ES7-277-0AA20-0XA0 EM 277 PROFIBUS DP module: -------------------------- - PROFIBUS DP slave module for CPU 226 and CPUs 222 and 224 with new order no. - 12 Mhz - One PROFIBUS DP port on the module - Dimensions: 71 mm x 80 mm x 62 mm (WxHxD) Siemens Industry Online Support - Automation Service, Automation ... |
Last edited by: Ste39 at: 7/3/2014 8:13 PMAdded document 0AA20 Last edited by: Ste39 at: 7/3/2014 3:48 PMIntegrate Last edited by: Ste39 at: 7/3/2014 3:47 PM |
|
This contribution was helpful to
|
|
Follow us on