Industry Online Support
Technical Forum
7/15/2014 2:26 PM | |
Posts: 1368 Rating:
|
Hello, the easiest way is the open communication with the T-Blocks. With this, you can communicate betweeh the PLCs via TCP/IP or UDP/IP. Have a look here https://www.automation.siemens.com/mdm/default.aspx?DocVersionId=41524141835&Language=en-US&TopicId=40600162315 There are also many FAQs and application available in the Portal. Edit: an Overview about the possibilities of PLC-PLC communication you find here http://support.automation.siemens.com/WW/view/de/78028908/0/en |
Last edited by: Pittiplatsch at: 7/15/2014 2:28 PM |
|
This contribution was helpful to
1 thankful Users |
7/15/2014 5:55 PM | |
Posts: 27 Rating:
|
Hello. My friend told me to change the IPs as folowed: PLC 1: 192.168.0.101 PLC 2:192.168.0.102 computer:192.168.0.1 When i tried it it worked. He said the first number(after last dot) has to be the same then the numbers doesnt matter. As i tried it it worked. I did not change anything else. I am having some troubles with the GET instruction now. I established the connection between the PLC-s with the GET instruction. Now i dont know what the adress of M0.0 in the PLC 2 is. Where can i check the address of M0.0 (M0.0 is type bool). I attacked the project. i appreciate your help, Jure AttachmentProject1.zip (137 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on