(0)| 8/21/2014 1:55 PM | |
|
Posts: 5225 Rating:
|
I do hope you are using MC_POWER also.. Yes you are right. The Q0.1 output can only be controlled via the motion control functions. The motion control command table will automatically decide the motion direction that you need. I recommend for you to have a look at the Siemens CE-X7 example [LINK] for a good sample to use as a starting point. Please also consider including jog motion control block. Then you have a way to control the motion in a manual way. To check that your motion is working correctly, use COMMISIONING tool. See the JPEG for detail. With this tool you can at least see if the motion can go forward and reverse. Greetings. w |
Follow us on