(0)| 8/27/2014 7:46 AM | |
|
Posts: 24 Rating:
|
Hi experts, Currently I've procured the following hardware (attached in pdf) and would like someone to confirm if either configuration are correct. I am very new to Sinamics therefore need some guidance. Thank you. AttachmentCLIQ and DC Link Config.pdf (235 Downloads) |
| 8/27/2014 8:00 AM | |
|
Joined: 5/12/2006 Last visit: 1/20/2026 Posts: 22829 Rating:
|
Hi, this config ist not possible. The Smart Line can only connect to one Control Unit not to two. Regards Christoph |
| 8/27/2014 11:24 AM | |
|
Posts: 24 Rating:
|
Do we need to connect the control unit to the smart line module? Or we can just have the smart line module to connect the motor power modules only? |
Follow us on