(0)| 8/31/2014 3:41 PM | |
|
Joined: 4/22/2010 Last visit: 3/31/2025 Posts: 5697 Rating:
|
Hello, Simatic Manager is part of the "classic" Step 7 and used to program S7-300 and 400 PLC's The latest version is Step 7 5.5 SP3. With this Version you can program your PLC for sure. Since you are learning i guess you want to buy a program for years to work with. Then maybe the new TIA portal V 13 is a better option. Then you can program not only the 300 and 400, but also the 1200 and 1500 series. Problem may be the CPU you have, if it's an oldy it can't be programmed in TIA. So please give us the partnumber (6ES7 314........) To get prices and more information you best contact your local Siemens rep. --> Contacts Worldwide I know there are some special offers for Students so ask for it. To try the TIA software, you can download a Trial version here: SIMATIC STEP 7 (TIA Portal) V13 TRIAL Download Hope this helps, Regards, Marcjan |
|
Problem solved? |
|
This contribution was helpful to
|
|
| 9/5/2014 4:04 PM | |
|
Posts: 4620 Rating:
|
Hello Bargathi, Our expert Marcjan had already sent to you representatives in the world. Contacts Worldwide Yes it is a representation in Malta enter and click the country. Your CPU Product data sheet 6ES7314-1AG14-0AB0 - Industry Mall - Siemens Programming package STEP 7 V5.5 + SP1 or higher or STEP7 V5.2 + SP1 or higher with HSP 218 |
Last edited by: Ste39 at: 9/5/2014 4:15 PMLast edited by: Ste39 at: 9/5/2014 4:12 PMLast edited by: Ste39 at: 9/5/2014 4:07 PMLast edited by: Ste39 at: 9/5/2014 4:06 PM |
|
| 12/31/2014 1:36 PM | |
|
Posts: 4758 Rating:
|
|
This contribution was helpful to
|
|
Follow us on